{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ION Enterprise v5.5 Management Console error: "This action cannot be completed because the other application is busy. Choose 'Switch To' to activate the busy application and correct the problem."

This is the error message that appears in the ION Enterprise Management Console:


Check the task manager and there are most likely multiple instances of managementconsole.exe, vista.exe, or designer.exe in the processes. You may also see multiple instances in the applications. This is most likely due to multiple users logged into the same programs. Either ending the other users session or rebooting the computer will resolve the problem.


Date Created: December 30, 2009
Last Revised: December 30, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200840 V1.0, Originally authored by MiNe on 12/30/2009, Last Edited by MiNe on 12/30/2009
Related ranges: ION Enterprise V5.5

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.