{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the waveform data stored in OS folder system of a PowerLogic SCADA server

Issue
Describe where to find waveform captures on the server where the Power Operations application resides

Product Line
EcoStruxture Power Operation 2023

Environment
EcoStruxture Power Operation

Cause
Waveform captures are placed in a seperate file folder/location from the rest of the software

Resolution
1. Go to PowerLogic SCADA user and data folder location. The default folder is as per below.
C:\Documents and Settings\All Users\Application Data\Schneider Electric\PowerLogic SCADA 7.10

2. Go to Data folder -> Cluster name of your current project -> your EMG device type -> port & board name -> your EMG device name in PowerLogic SCADA -> waveforms

Example
C:\Documents and Settings\All Users\Application Data\Schneider Electric\PowerLogic SCADA 7.10\Data\cluster\sepam40\port1_board2\s1_b1_d1_p1\waveforms
File Location example image

Schneider Electric Nigeria