{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Reverse the Logic of a Digital Value in PowerLogic SCADA v7.10 (PLS)

Goals and Symptoms

How to reverse the logic of a Digital value in PLSCADA?

Causes and Fixes

To reverse the logic of a digital value in PL SCADA, use a NOT in front of the Variable Tag in the expression box where the tag name is used.
A NOT can be used to reverse the logic for an Alarm, specifically, when a digital device has a Normally On state (1), and is actually in alarm only when the value is Zero (the OFF state).

The screen capture below shows an example of using NOT in the Variable Tag A field of a Digital Alarm:


The following capture is an example of a Genie utilizing reversed logic. In this case, the graphic symbol will be hidden as long as the substituted variable tag is equal to one.


Legacy KB System (APS) Data: RESL203760 V1.0, Originally authored by AnVa on 10/22/2010, Last Edited by AnVa on 10/22/2010
Related ranges: PowerLogic SCADA 7.1

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.