{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can Total Demand Distortion (TDD) be manually calculated?

Total Demand Distortion (TDD) can be calculated by the following two methods.
*Note you will need the Peak Demand Current.

1) If the per phase THD and Fundamental currents are known, the attached calculation can be used.

Image 1


2) If the per phase thd and true RMS currents are known, the attached calculation can be used.
Image 2

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: