{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The port is in use or an attempt was made to access a socket in a way forbidden by its access permissions." when starting PowerLogic SCADA Runtime

Goals and Symptoms

The following error message appears in PowerLogic SCADA (PLS) v7.10 after starting Runtime:
Cannot Open Server <ServerName>. The port is in use or an attempt was made to access a socket in a way forbidden by its access permissions.

As a result, the IO Server will not start.

Causes and Fixes

The default port used by the I/O Server is 2078. The above issue can be resolved by assigning a different port to the IO Server in the Servers > I/O Server field in the Project Editor.



For a complete list of default ports used in PLS, refer to the System Integrator Manual (search for 'default port'). Here are a few:

2075 Reports server communications
2076 Alarm server communications
2077 Trends server communications
2078 Legacy I/O communications
2082 Publish subscribe I/O server communications

To determine which ports are already in use, open a Command Prompt window and run the command 'netstat -a'. This will list all of the TCP port numbers currently in use in the system.

For additional information, refer to RESL197082.

Keywords: PLSCADA, PL SCADA, PowerSCADA, Power SCADA, StruxureWare PowerSCADA Expert, SPE 7.1, 7.2, 7.10, 7.20, net stat


Legacy KB System (APS) Data: RESL209208 V1.0, Originally authored by AnVa on 09/27/2012, Last Edited by AnVa on 09/27/2012
Related ranges: PowerLogic SCADA 7.1, PowerSCADA Expert 7.2

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.