{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Excitation (aka Wake up or Minimum Pickup) Current for the PM800 Series

The PM800 meets IEC620583 which dictates that the minimum pickup current is 5 mA. There must be a minimum of 5 milliamps current on the CT secondaries (0.1% load with a 5 amp secondary, or 0.5% load with a 1 amp secondary) for the meter to begin metering current.
Key Words:
excitation, pickup, pick up, turn on, PM820, PM850, PM870, PM8

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.