{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When Paralleling CTs on a PowerLogic Energy Meter, PM800, CM3000, or CM4000 does the data report separately or as a combined total?

Issue
Data values from paralleled CT's

Product Line
PM800
CM3000
CM4000

Environment
Hardware

Cause
Data signals on the same line

Resolution
These meters monitor the Parallel CTs as a single combined total rather than as separate connection points. The meter will provide a combined total for the energy accumulation rather than a total per set of CTs.

Schneider Electric Nigeria