Search FAQs
Is there a Mounting Adapter available to retrofit a Series 4000 Circuit Monitor in place of a Series 2000 Circuit Monitor or CM100/200 Series meters?
Issue:
Need to retrofit CM4000 meter in place of existing CM2000 or CM100/200 Series Meters, but the form factor is a different size.
Product Line:
CM100, CM150, CM200, CM250
CM2000, CM2050, CM2150, CM2250, CM2350, CM2450
CM4000, CM4250, CM4000T
Environment:
Power meter retrofit and replacement
Cause:
A customer wishes to replace obsolete CM2000 or CM100/200 series meters with CM4000 Series meters.
Resolution:
A mounting plate adapter is available that will allow a user to install a CM4000 series meter in an existing cutout for a CM2000 or CM100/200 series meter. "CM4MA" is the mounting adapter part number. This part is a filler plate used when mounting a Series 4000 Circuit Monitor (CM4) where a 2000 Circuit Monitor (CM2) was removed. The same mounting adapters designed to be used with the CM2000 series meters will also work with the CM100, CM150, CM200, and CM250.
See attached document for more information.
Need to retrofit CM4000 meter in place of existing CM2000 or CM100/200 Series Meters, but the form factor is a different size.
Product Line:
CM100, CM150, CM200, CM250
CM2000, CM2050, CM2150, CM2250, CM2350, CM2450
CM4000, CM4250, CM4000T
Environment:
Power meter retrofit and replacement
Cause:
A customer wishes to replace obsolete CM2000 or CM100/200 series meters with CM4000 Series meters.
Resolution:
A mounting plate adapter is available that will allow a user to install a CM4000 series meter in an existing cutout for a CM2000 or CM100/200 series meter. "CM4MA" is the mounting adapter part number. This part is a filler plate used when mounting a Series 4000 Circuit Monitor (CM4) where a 2000 Circuit Monitor (CM2) was removed. The same mounting adapters designed to be used with the CM2000 series meters will also work with the CM100, CM150, CM200, and CM250.
See attached document for more information.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: