{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can setpoint modules be configured from the Dashboard view in Power Monitoring Expert (PME) Web Applications?

Issue
Is it possible to configure the setpoint module from the Web Applications Dashboards tab?

Product Line
Struxureware Power Monitoring Expert 7, 8.x, 9, 2020

Environment
Web Applications - Dashboard Tab

Resolution
No.  Setpoint modules can only be set up and modified in PME Designer, PME Vista, or ION Setup software.

Schneider Electric Nigeria