Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 7.x.x
Struxureware Power Monitoring 7.0.1
ION Enterprise
Cause
User would like to view the data points from a waveform capture using PME, SPM, or ION
Resolution
1. Open the waveforms in the Vista Diagram for the meter.
2. Highlight the value to be plotted and click the "plot" button in the toolbar.
3. Right click on the plotted Waveform and select V1 --> Data (other values selected will be labeled accordingly e.g. V2, V3, I1, etc...)
4. Select all the data points and click the Copy button and Paste into Excel.
Please see the following video for walk through instructions.
Released for:Schneider Electric Nigeria