Search FAQs
How do I add ION8650 Support in ION Enterprise 6 ?
Issue
ION 6 does not include an ION8650 driver natively, user wishes to add the native driver to the ION Enterprise system.
Product Line
ION Enterprise 6
Environment
Driver Install
Cause
ION8650 came out after ION Enterprise 6 and was not part of the software during release.
Resolution
In order to add ION8650 support in ION Enterprise 6 you will need to run the linked ION8650 device updater on the primary ION Enterprise 6 server.
You can download the device updater from the global Schneider Electric Website at the following link below
https://www.se.com/hk/en/download/document/ION8650_Device_Updater/
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: