{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are the 3090SCCT series current transformers rated for outdoor use?

Product Line
3090SCCT

Environment
Durability

Resolution
The 3090SCCT series current transformers are not rated for outdoor use.

Schneider Electric Nigeria

Explore more
Range:
EM4000 seriesActi 9 iEM3000Current transformer T1
Explore more
Range:
EM4000 seriesActi 9 iEM3000Current transformer T1
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.