{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the correct order to upgrade the exec in the Quantum Unity processor 140CPU651x0?

1. Processor Operating Systems are upward compatible: updating a processor with a higher Operating System version is always allowed

2. It is recommended to always upgrade the OS version of a processor with the latest available version

3. It is recommended that the Copro version is associated with the OS version indicated in the QUANTUM - Launch History tables (mandatory for HotStandby Systems)

4. It is mandatory to upgrade the Ethernet Coprocessor before the Processor OS

5. It is not recommended to downgrade the OS of a Processor


Schneider Electric Nigeria