{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the RJ45 Modbus RS232 ports of the TSXETG100 and the 174CEV30020 have the same pinout?

No the RJ45 Modbus RS232 ports of the TSXETG100 and the 174CEV30020 do nothave the same pinout.
The pin assignments of the ports are as follows:


Schneider Electric Nigeria