{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What pin out can be used for Momentum RJ45 to RJ45 RS232 Modbus communications?

Cabling scheme for the RJ-45-(8x8) to RJ-45-(8x8) (null modem);


  • This pin out is to be used for Momentum to Momentum RS232 connection only (XMIT/XXMIT).
texttext
texttext

Legacy KB System (APS) Data: RESL192681 V1.0, Originally authored by RoAl on 09/03/2008, Last Edited by RoAl on 09/03/2008
Related ranges: Modicon Momentum

Schneider Electric Nigeria