{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
In Vijeo Designer, can I call a bit of a word in the expression editor of a lamp or push button object?

Issue:
Calling a bit of a word in the expression editor of a lamp or push button object


Product Line:
Vijeo Designer


Resolution:
Yes, you can extract a bit of a word in Vijeo Designer from the expression editor of the lamp or push button's lamp field. The syntax
in the expression editor are as follows: VariableName.X(n) where n = bit position
For example: If I want to display the bit 0 of an integer variable INT01 the syntax would be, INT01.X(0) in the expression editor.

Note:
-This method does not work with elements of array, structure, folder, recipe group, and block variables.
-If the variable is in a folder (for equipment scan groups for example), you cannot use the bit referencing... eg. MyFolder.MyVariable.X(0) does not work

Schneider Electric Nigeria