Search FAQs
What operating systems is PowerLogic ION Setup 2.2 supported on?
Issue:
User may need to install ION Setup 2.2 and wants to know if it will run correctly on their operating system
Product Line:
ION Setup 2.2
Environment:
Meter Configuration Software
Resolution:
PowerLogic ION Setup is supported only on Microsoft based operating systems. Below is a summary of the operating systems that are supported.
PowerLogic ION Setup v2.2 is fully supported on the Microsoft operating systems below.
- Windows 98
- Windows 2000 and 2000 server
- Windows XP
- Windows 2003 Server
They are not officially supported however PowerLogic ION Setup should work as long as the application is installed and run with a user that has administrator access(can access the registry).
No official testing at this time has been done nor scheduled for version 2.2 on these operating system.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: