{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which measurements are used by the Energy Cost and Load Profile reports?

Issue
The Energy Cost and Load Profile reports require that data is logged to specific measurements in order to run.

Product Line
ION Enterprise 6.0 SP1
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0

Environment
Web Applications Reports

Cause
The Energy Cost, and Load Profile reports have a list of possible measurements that it looks for in a specific order. The default order is indicated below, but note that the order can be configured or additional measurements can be added via a SQL query or by editing the view directly in Management Studio. This list of measurements is read from the database its an entry in vCFG_ConfigItems (a view in ION_Network)

Resolution
Energy Cost Report:

kWh:
Active Energy Delivered-Received - ID135
Active Energy Delivered+Received - ID198
Active Energy Delivered ID129
Active Energy Received Rate A ID130
Active Energy Delivered Interval ID134
Active Energy Received Interval ID144

MeasurementIDLabels Mapped To This Measurement
135kWh del-rec
kWh net
Real Energy Signed
Real Energy
198kWh del+rec
kWh tot
Real Energy Absolute
129kWh del,
kWh imp, kWh
kWh tot del
Real Energy into the Load
130kWh del A
kWh del tariff 1
134kWh del int
kWh imp int
Real Energy Delivered Interval
144kWh rec int
kWh exp int
Real Energy Received Interval


kVARh:
Reactive Energy Delivered-Received ID97
Reactive Energy Delivered + Received ID191
Reactive Energy Delievered ID91
Reactive Energy Received Rate A ID92
Reactive Energy Delivered Interval ID96
Reactive Energy Received Interval ID106
Measurement IDLabels Mapped To This Measurement
97kVARh del-rec
kVARh net
Reactive Energy Signed
Reactive Energy
191kVARh del+rec
kVARh tot
Reactive Energy Absolute
91kVARh del
kVARh imp
kVARh
Reactive Energy Into the Load
92kVARh del A
kVARh del tariff 1
96kVARh del int
kVARh imp int
106kVARh rec int
kVARh exp int

kVAh:
Apparent Energy Delivered + Received ID63
Apparent Energy Delivered-Received ID740
Apparent Energy Delivered ID489
Apparent Energy Delivered + Received Rate A ID2659
MeasurementIDLabels Mapped To This Measurement
63kVAh
kVAh del+rec
kVAh tot
Apparent Energy
740kVAh net
kVAh del-rec
489kVAh del
kVAh imp
2659kVAh tariff 1


kW:
Active Power Sliding Window Demand Delivered-Received ID107
Active Power Sliding Window Demand Delivered+Received ID738
Active Power Sliding Window Demand Delivered ID116
Active Power Thermal Demand Delivered-Received ID117
Active Power Sliding Window Demand Received ID739
MeasurementIDLabels Mapped To This Measurement
107kW sd del-rec
kW swd
kW tot swd
kW Dmd del-rec
Demand Real Power Sliding
Demand Real Power
738kW sd del+rec
116kW demand
kW sd del
kW tot SD
117kW td del-rec
Demand Real Power - Thermal
739kW sd rec

kVAR:
Reactive Power Sliding Window Demand Delivered Received ID69
Reactive Power Sliding Window Demand Delivered+Received ID735
Reactive Power Sliding Window Demand Delivered ID78
Reactive Power Thermal Demand Delivered-Received ID79
Reactive Power Sliding Window Demand Received ID737
MeasurementIDLabels Mapped To This Measurement
69kVAR sd del-rec
kVAR swd
kVAR Dmd del-rec
Demand Reactive Power Sliding
Demand Reactive Power
735kVAR sd del+rec
78kVAR demand
kVAR sd del
kVAR tot SD
79kVAR td
kVAR td del-rec
Demand Reactive Power - Thermal
737kVAR sd rec

kVA:
Apparent Power Sliding Window Demand Delivered+Received ID37
Apparent Power Sliding Window Demand Delivered-Received ID736
Apparent Power Sliding Window Demand Delivered ID573
Apparent Power Thermal Demand Delivered+Received ID47
MeasurementIDLabels Mapped To This Measurement
37kVA sd del+rec
kVA swd
kVA Dmd
Demand Apparent Power - Sliding
736kVA sd del-rec
573kVA demand
kVA sd del
kVA tot SD
Demand Apparent Power
47kVA td

Load Profile Report:

Active Demand:
Active Power Sliding Window Demand Delivered-Received ID 107
Active Power Sliding Window Demand Delivered+Received ID 738
Active Power Sliding Window Demand Delivered ID 116
Active Power Thermal Demand Delivered-Received ID 117
Active Power Sliding Window Demand Received ID 739
MeasurementIDLabels Mapped To This Measurement
107kW sd del-rec
kW swd
kW tot swd
kW Dmd del-rec
Demand Real Power Sliding
Demand Real Power
Panel-Main Demand Real Power
738kW sd del+rec
116kW demand
kW sd del
kW tot SD
117kW td del-rec
Demand Real Power - Thermal
739kW sd rec

Reactive Demand:
Reactive Power Sliding Window Demand Delivered Received ID 69
Reactive Power Sliding Window Demand Delivered+Received ID 735
Reactive Power Sliding Window Demand Delivered ID 78
Reactive Power Thermal Demand Delivered-Received ID 79
Reactive Power Sliding Window Demand Received ID 737
MeasurementIDLabels Mapped To This Measurement
69kVAR sd del-rec
kVAR swd
kVAR Dmd del-rec
Demand Reactive Power Sliding
Demand Reactive Power
735kVAR sd del+rec
78kVAR demand
kVAR sd del
kVAR tot SD
79kVAR td
kVAR td del-rec
Demand Reactive Power - Thermal
737kVAR sd rec

Apparent Demand:
Apparent Power Sliding Window Demand Delivered+Received ID 37
Apparent Power Sliding Window Demand Delivered-Received ID 736
Apparent Power Sliding Window Demand Delivered ID 573
Apparent Power Thermal Demand Delivered+Received ID 47
MeasurementIDLabels Mapped To This Measurement
37kVA sd del+rec
kVA swd
kVA Dmd
Demand Apparent Power - Sliding
KVA SD
736kVA sd del-rec
573kVA demand
kVA sd del
kVA tot SD
Demand Apparent Power
47kVA td
kVA td del+rec
Demand Apparent Power - Thermal


Power: for devices that don't do SWD
Active Power ID193
Reactive Power ID187
Apparent Power ID544
MeasurementIDLabels Mapped To This Measurement
193kW tot
kW total
Real Power Total
187kVAR tot
kVAR total
Reactive Power Total
544kVA tot
kVA total
Apparent Power Total

Schneider Electric Nigeria