Search FAQs
What is the maximum number of nodes allowed on one Profibus network?
The maximum number of nodes per bus for a Profibus network is 32 without repeaters.
125 nodes may be used with 3 repeaters and 4 network segments.
They can be addressed 1-126.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: