{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the SCR Snubber part number for an ATV61HC16N4 thru ATV61HC63N4 or ATV71HC13N4 thru ATV71HC50N4 drives?

Issue:
What is the SCR snubber part number for an ATV61/71 drive?

Product Line:
ATV61 and ATV71

Environment:
All serial numbers for ATV61 and ATV71

Cause:
Part number needed to order part.

Resolution:
VX4A1200 for Frame sizes 11 - 15
ATV61HC16N4 thru ATV61HC63N4 or ATV71HC13N4 thru ATV71HC50N4?

Schneider Electric Nigeria