Search FAQs
Should address 199 be assigned to a CM2000 meter?
Issue
A CM2000 can be assigned an address from 1-199; however, should address 199 be used?
Product Line
CM2000 Series
Environment
Meter Addressing
Resolution
Address "199" should always be reserved. The circuit monitor will accept 199, but this is the address that the Circuit Monitor defaults to in a failure situation.
For steps on setting the CM2000's device address, please refer to FA218954.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: