{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Resetting the Circuit Monitor 2000 Series (CM2000) to Factory Defaults (Master Reset)

Issue
Need to reset the Circuit Monitor Series 2000 back to the factory default settings.

Product Line
CM2000 Series

Environment
Programming

Resolution
This should always be the last resort.
Reseting the meter will clear the CT/PT ratios, System Type, I/O setup, Alarms/Events, Data Logs, Event logs, Waveform Capture Logs, and etc.
The device address and baud rate are not reset on versions 14.000 or later.

The attached article explains how to reset the CM2000 to factory default

Schneider Electric Nigeria

Attachment(s)
Resetting_the_CM2000_to_Factory_Defaults.pdf [17.92 KB]