{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I activate/deactivate revenue security on the CM3000/CM4000?
Issue
Activating revenue security on the CM3000/CM4000

Product Line
CM3000
CM4000

Environment
Security

Cause
Activating the revenue security will protect against other users changing any settings.

Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.

To activate revenue security for the first time the revenue security button needs to be enabled and then it needs to be activated.

To enable the revenue security button you will need to use a Modbus Testing utility and write the decimal value 1411 to register 8000.

After the button is enabled it must be activated by pressing the button again.

This button is accessed by powering down the meter and removing all I/O modules
i/o Extender
Next power the meter back up. The circuit monitor must have power in order to activate revenue security. Open the access door by sliding the door along the side of the circuit monitor then gently pull the door down to open it. Clips
Finally discharge all static electricity by placing your hand on any grounded metal surface. Press and hold the security button for a few seconds until the security LED is lit.
Button

To deactivate revenue security hold the revenue security button down until the red light inside the compartment turns OFF.

To disable the revenue security button write the value 1410 to register 8000.

For a more complete step by step procedure please see the attached CM4000 Installation Manual and follow the steps beginning on page 28

Schneider Electric Nigeria

Attachment(s)
CM4000_Install_Manual.pdf [9.03 MB]