{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of the EMFP fuse pack assembly and does it come with any mounting hardware?

Issue
A user may want to know the dimensions of the fuse holders and their respective lead lengths

Product Line
Energy Meters

Environment
Meter Installation

Cause
There may be the need to ensure that the fuse holders will fit in a given space and whether the leads are long enough for the location of the meter and the source.

Resolution
The fuse pack is 2.5 inches long and 1 inch in diameter. The conductor is 18 inches long on both sides of the fuse pack.
See picture below of a single fuse holder:

Schneider Electric Nigeria