Search FAQs
Video: Updating DST Settings for Meter Clock using ION Setup
Issue
Updating daylight savings time (DST) settings for PowerLogic ION power meter clocks via ION Setup.
Product Line
PM8000
ION8650
ION8600
ION7650, ION7550
ION7600, ION7500, ION7400
Environment
ION Setup 3.0
Cause
Updating DST Settings for meter clock using ION Setup. This is much easier than using ION Designer, in particular, there is no need to predetermine the DST Start and End dates.
Resolution
- Determine the physical location of device and the respective Time Zone (for UTC adjustment).
- Using Setup Assistant to set the time zone setting for the clock module.
- Edit remaining settings for the clock module (refer to Time Synchronization & Timekeeping technical note).
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: