{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Display a Register Handle in a Meter Using ION Setup

KB Article
Summary

This article describes how to configure a Meter display using ION Setup 2.0 to show any ION Handle.


Keywords

ION Setup V2.0, handle, display


Resolution

  • 1. Find the ION handle for the register that is to be displayed in the Meter.  See KB article 10685 for more information.
    2. Right-click applicable meter, select Properties, select Show Advanced ION Setup.


    3. Select display module to be changed, or add a new display module (if necessary).
    4. Enter handle into Parameter field.
    5. Hit Search, OK, Send

Schneider Electric Nigeria