{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to send a Master Reset to an EGX100, EGX300, EGX200 or EGX400.

Article available in these languages: Spanish

Issue
Master Reset to an EGX100, EGX300, EGX200 or EGX400 gateways are needed to be done remotely through register write.

Enviroment
EGX100
EGX200
EGX300
EGX400

Resolution
A master reset to an Ethernet Gateway (EGX) will reset all settings to the manufactures default settings including the IP address.
For the EGX100 and EGX300, the default IP address is 169.254.0.10. For the EGX200/400 it is 10.10.10.10.

Modbus Tester software or some other Modbus TCP/IP program (like Modscan) can be used to send the master reset register write.

For the EGX100 and EGX300 use address 254 and write decimal 9030 to register 2800.
For the EGX200 and EGX400 use address 254 and write decimal 17476 to register 8000.

Once you have sent this register command to the EGX you will have to cycle power to reboot the processor.


Image 1
If you don´t know the IP address, then please refer to FA212273 "How to determine the IP address of an EGX/ECC gateway" for further support

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.