Issue:
The end user would like to extend the length of cables attached the a Current Transformer on a BCMSC meter.
Product Line:
Branch Current Monitor Split Core (BCMSC)
Environment:
Current Transformer for BCMSC
Cause:
The monitoring source may be beyond reach of the Current Transformer that comes standard with the BCMSC.
Resolution:
The split core current transformers can be extended to a maximum distance of 20 feet. The recommended wire size is 10 gauge (AWG).
Released for:Schneider Electric Nigeria