{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Error message received when downloading sft2841 v10 - "Cannot download msvcrt.dll". How to solve this issue?

This error is caused by an incorrect uninstallation of SFTv9. If the client uninstalls the software manually (without add/remove programs), the software will not completely delete all 'dlls' and conflicts will arise whenever performing upgraded installations. In order to solve this issue, manually install the msvcrt.dll file on the cd before performing the complete SFT2841 installation.


AEDL3


  • Re-published to revised security level: 16 June 2008 by DRM

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188972 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/18/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)

Schneider Electric Nigeria