{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does there exist a USB to RS-232 converter for the SFT2841 software (and Sepam mini-DIN front port connection)?


It is recommended to use Telemecanique's converter TSXCUSB232 since this uses the driver already installed by SFT2841.

Up to SFT2841 V10.1 Com port from 1 to 4 only should be used for Sepam 40 ( 1 to 9 available but if >4 user messages and logical equation will not be loaded ).

Starting with Version 10.3 available Q4 2008 all com port allowed by operating system will be usable.

AEDL3


  • Last updated: 13 June 2008 by DRM

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188982 V2.0, Originally authored by KBAdPM on 11/08/2007, Last Edited by DaMi on 06/14/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.