Search FAQs
TCPOpen library setup returns the error 'The LibPath was not found in registry'
Issue
TCPOpen library setup returns the error 'The LibPath was not found in registry'.
Product Line
TLXCDTCP50M
Unity Pro XL v4.0
Environment
Windows 7, Unity
Resolution
Setup returns the error: The LibPath was not found in registry.
The following is from the Unity 'Readme:
2.7. TCP Open library and Unity Dif libraries
Organization of data stored on the computer has changed with Unity Pro V4.0. To use some companion with Unity Pro, it is necessary to use the last version of these software packages, TCP Open library version V2.20 and Unity Dif version V2.0 SP2 min.
The problem can be resolved by using the following resolution.
- Insert the Unity Pro V4.0 CDROM. (Cancel autorun if necessary. )
- Locate the file named UpdateForCompanions.bat in the folder named UpdateForCompanions .
- Click on Start\Programs\Accessories\Command Prompt to open a DOS window.
- Change the directory in the DOS window to the path for the CD-ROM drive. (i.e., type F:) at the prompt F:\>, enter cd UpdateForCompanions
- At the command prompt F:\UpdateForCompanions>, enter 'UpdateForCompanions' followed by the letter corresponding to the installed Unity Pro package: "S", "M", "L", "XL"
.i.e.,
G:\UpdateForCompanions>UpdateForCompanions XL
- Wait for the update to finish.
- Run the TCP Open setup.
Legacy KB System (APS) Data: RESL199375 V1.0, Originally authored by AlCh on 12/15/2009, Last Edited by AlCh on 12/15/2009
Related ranges: ConneXium - Ethernet
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: