Issue
Quick start for configuring the 'TCSEGDB23F24FA' M340 Modbus Plus Proxy Module
Product Line
'TCSEGDB23F24FA' M340 Modbus Plus Proxy Module
Environment
Windows 7
Resolution
The following steps can be used to configure the' TCSEGDB23F24FA' M340 Modbus Plus Proxy
Module
- Set the Modbus Plus address for the bridge using the rotary switch that are located on the back
- Connect to the module using the default MAC derived ethernet address.
- Enter the default username (USER) and password (USER) to access the configuration/setup
- Click on 'Setup'.
- Click on 'IP Setup'.
- Enter the IP address parameters.
- Click on 'Apply'.
- Click on 'Save To Flash'.
- Click on 'IP address' under the section labeled 'M340 Interface'.
- Enter the IP address parameters.
- Click on 'Apply'.
- Click on 'Save To Flash'.
- Click on 'Register Offsets' under the 'M340 Interface' section.
- Fill in the appropriate parameters.
- Select 'Legacy Compatability 0x 4x by 1' if you are communicating to a Modicon PLC.
- Click on 'Apply'.
- Click on 'Save To Flash'.
- If applicable, click on the appropriate sections to be filled in under the section named 'Modbus Plus Peer Cop'
Released for:Schneider Electric Nigeria