{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Timestamps Displayed in the Different Components of ION Enterprise and ION Devices

Goals and Symptoms

This article explains how ION Enterprise and ION devices display timestamps.

Facts and Changes

Real-time data
Historical data

Timestamp

WebReach

Vista

Reporter

Clock module

Causes and Fixes

All timestamps are stored in the database by ION Enterprise using UTC format. However, different settings are used to display real-time and historical data, which may confuse the user.

Vista

For real-time data, Vista displays the meter time in local time according to the time zone settings of the client's operating system. For historical data, Vista displays the timestamps as calculated using the server operating system's time zone settings (assuming the option Show Logs in Universal Time (UTC) is unchecked).

Reporter

Reporter, like Vista, applies the time zone offset settings on the local PC to the UTC time to get the Local Time column.

WebReach

For real-time data screens, WebReach displays the meter time in local time according to the meter (i.e. according to the time zone settings on the meter). For historical data, WebReach displays the timestamps as calculated using the server operating system's time zone settings.

ION Devices Front Panel

The time zone settings on the meter (in the Clock module) allow the meter to display the local time.

  • Original article#10767

    Public

    All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188928 V1.0, Originally authored by KBAdPM on 11/07/2007, Last Edited by KBAdPM on 11/07/2007
Related ranges: ION Enterprise V5.5

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.