{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The PQ report in ION Enterprise 5.6 SP1 does not include meter transient events. What can be done to resolve this?

There is a HOT FIX for ION:E 5.6 SP1 to re-add the missing transient subsection of the PQ Report.
The full list of repairs in the HOT FIX are below:

- Fix to Power Quality report template so that transient events are included
- Fixes to the Load Profile, IEC6000-4-30 reports, and EN50160 templates so that those reports will work with the new charting engine in Excel 2007
- Elimination of the 'compatibility warning' dialog, which appears for any report when the user attempts to save it if they are using Excel 2007

Please download this hotfix from here (http://www.global.powerlogic.com > Support > ION Enteprise > Hotfixes)/

  • Last Revised: 4 June 2008

    Applies To: ION Enterprise 5.6 SP1

    Original Author: LS

    Public

    All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL192092 V1.0, Originally authored by KBAdPM on 06/05/2008, Last Edited by KBAdPM on 06/05/2008
Related ranges: ION Enterprise V5.6

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.