{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How long can the overvoltage condition last on the metering inputs of the Series 4000 Circuit Monitor (CM4000)?

Issue
Limits of the CM4000 overvoltage conditions

Product Line
CM4000

Environment
Product Specifications

Cause
Over voltage conditions that the CM4000 can sustain before failure

Resolution
From Table B-1 of Appendix B in the CM4000 reference manual, the meter allows a 50% metering over-range of voltage. The meter can handle this overvoltage condition indefintely.

Schneider Electric Nigeria

Attachment(s)
CM4000_Reference_Manual.pdf [3.41 MB]