The ION6200 can measure V L-L Avg as well as V L-N Avg, however in delta mode, since there is no neutral, V L-N Avg is not available. What is shown on the front panel display is V L-L Avg and it is labeled V Avg. The meter's firmware is designed to display this quantity on the front panel. Having said that, V L-N Avg is available through Modbus or ION protocol with any ION software.
Date Created: June 13, 2008
Last Revised: February 16, 2009
Public
Original Author: KG
All content © 1992-2009 Schneider Electric
Legacy KB System (APS) Data: RESL197835 V1.0, Originally authored by KBAdPM on 02/17/2009, Last Edited by KBAdPM on 02/17/2009
Related ranges: ION6200
Released for:Schneider Electric Nigeria