{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
170AMM11030 Analog Outputs May Not Function Properly.

Issue
The purpose of this Resolution is to inform users of 170AMM11030 Momentum I/O bases of a problem with the analog outputs after operating for a short time.

After 3-4 minutes of module operation, the actual analog outputs for channels 1 & 2 are different from their expected values. Negative output voltages may occur when a positive voltage is expected.


Product Line
Momentum
170AMM11030


Resolution
A firmware and hardware solution has been implemented. Modules with an SV of 1.12 and a PV04 have this fix (implemented 9/04).

This is not a field upgradable option. Modules that are experiencing the issue described above must be exchanged.


Legacy KB System (APS) Data: RESL164814 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum I/O

Schneider Electric Nigeria