{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a script in Vijeo Designer that will allow me to write a new IP address of an Equipment at Runtime?

Issue:
Writing a new IP address of an Equipment at Runtime in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
Yes, you can write the IP address of an equipment via scripting. This feature was implemented in Vijeo Designer V5.0 SP1. This code will set IP Addresses for any driver, not just the Modbus driver. Below is an example script:


  • // --------------- Write some data -----------------------------------------

    // Length is given by NewIP_InputData.length

      • int [ ] NewIP_InputData = {10, 187, 225, 135};

        ModbusEquipment01.openConfig();

        ModbusEquipment01.setProperty( "Con_IPAddress", NewIP_InputData );

        ModbusEquipment01.commitConfig();


Schneider Electric Nigeria