undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Wiring of RS485 Communications Networks

Issue
This document attempts to explain correct methods of wiring RS485 communication networks in industrial environments based on various application notes and technical articles.

Environment
RS485 Serial Modbus Communications

Resolution
1. RS-485 (EIA/TIA-485) Differential Data Transmission System Basics

The RS-485 standard was developed jointly by two trade associations: the Electronic Industries Association (EIA) and the Telecommunications Industry Association (TIA). The original prefix "RS" stands for Recommended Standard and has been officially replaced with "EIA/TIA" to help identify the origin of its standards.

RS-485 Standard Specifications
Mode of operation
Differential
Allowed no. of Tx and Rx
32 Tx 32 Rx
Maximum cable length
4000ft length
Maximum data rate
10Mbps
Minimum driver output range
±1.5V
Maximum driver output range
±5V
Minimum drive capability
±55mA
Maximum driver short-circuit current
250mA
Tx load impedance
54
Rx input sensitivity
±200mV
Maximum Rx input resistance
12k
Rx input voltage range
-7V to +12V
Rx logic high
>200mV
Rx logic low
<200mV
Max common mode voltage
-7V to +12V


Full duplex implementation requires 4 wires. This may be necessary for some applications involving legacy devices. In half-duplex implementation 2 wires are used this is the recommended configuration for most Schneider Electric PMC devices.
All products manufactured by Schneider Electric PMC support half-duplex, 2 wire configuration. The 4 wire interface is usually implemented in order to avoid creating a T (tee) or star connections or to support full duplex connections.
A twisted pair type of cable should be used in order to reduce radiated emissions and improve immunity of the communications system to any external electromagnetic interference.
The National Electrical Code and all applicable local regulations must be followed when installing the communications wiring.

Cable examples:
  • Belden 9841 or Alpha 6412 or equivalent cable may be used for applications under 300V that are indoors or outdoors in conduit above grade.
  • Belden 3074F or equivalent cable may be used for applications greater than 300V which are indoors or outdoors in conduit above grade.
In all devices the RS485 ports are opto-isolated from the internal device electronics. All devices with RS485 port have a shield terminal, which may be connected to the chassis ground (e.g. on 7X50, 880, 8600) or to the isolated reference of the RS485 port (i.e. no connection to the chassis ground as in 6200, 6300, 6100)

2. Network Configuration
2.1 Topology
Several types of network topologies are possible, but the daisy-chain bus configuration is the most efficient. Typically, one of the units is the client controlling the network traffic and prevents multiple drivers from being active at the same time (bus contention). A shielded twisted pair cable is the physical medium. The cable impedance should be within 100-120ohm range. In the Backbone with Studs technology, no studs should be left unconnected at the device end. Otherwise, such a stud will act as an antenna and introduce a significant amount of noise on the RS485 bus, to such a point that communications may become impossible. This is actually a fairly common source of problems.




The longer the cable, the lower the data rate:
2.2 Termination
Termination resistors that match the cable's characteristic impedance are essential for minimizing reflections and consequently communication error rates and electromagnetic emissions. For common RS-485 cables (a twisted pair of 24AWG wires), this means a 100-120 resistor at both ends . Termination resistors should be used especially with long cable length to ensure data integrity. Note that, on very long cable length, adding termination resistors can sometime cause an additional drop of voltage that will cause a loss of communication on the devices that are furthest from the client. In this case, adding a repeater or removing some termination resistors can restore communications.

2.3 Fails-Safe Biasing
Open bus condition:
When a node is disconnected from the bus, the state of the bus, as seen by the  receiver, is undetermined and may result in random output from the receiver.  A weak failsafe biasing is recommended to ensure that the receiver does not enter undetermined state under open bus conditions.

Idle bus condition:
When no drivers are active on a bus with termination resistors, those resistors will decrease the differential bus voltage to zero, which according to the RS485 standard, is an undefined bus condition. Biasing resistors should be used in order to generate a valid bus logic state under idle-bus conditions. Biasing resistors are only needed at one node (usually the client), hence configuration switches must be used if the biasing resistors are incorporated into every node. Only one device on the bus should be providing the biasing. The biasing resistors may be external or internal to the device. Some products e.g.8800, 7X50 have internal resistors which may be connected with internal switches to provide biasing of the bus.  The Com 32 and Com 128 have permanently connected biasing resistors.

2.4 Unit Load (U.L.)
A one RS485 transceiver represent a load of 1U.L. The RS485 standard specifies the bus loading as 32 U.L.

2.5 Shielding and Grounding
The RS485 interface standard does not specify a ground wire, but such wire is needed to provide a return path for common mode currents and consequently reduce emissions. It may be possible to operate the RS485 loop without a ground wire, but such systems may radiate high levels of EMI.

A shield limits coupling of external interference and noise onto the bus. Generally the shield should be connected to the chassis ground (installation ground) at one end of the cable. In case of ground potential differences between nodes (common in industrial locations) this arrangement prevents the flow of DC ground loop currents in the shield. Ground loop currents flowing in the shield will induce noise in the communications cable. A capacitor or an RC network may be used between the other end and ground.



The RS485 nodes can tolerate from -7V to +12V  of common mode voltage. When this voltage is exceeded the nodes are no longer guaranteed to function and may even be damaged.
Due to significant differences in ground potentials that may and will be present between nodes in industrial locations, ground should not be used as a reference. In installations where ground is used as return path 100-120 resistors may be used to limit the ground currents flowing due to ground potential differences between devices.
The figure below illustrates the grounding concepts.


Connection Example: 6300 meter, terminated daisy chain bus.

The shield terminal is not connected to chassis ground of the meter. Installer must ensure low impedance connection to the system ground at one end of the cable. The 4 wire port on the 6300 is intended to help the installer avoid making T (or stub) connections.  Note the use of termination resistors RT.

texttexttexttext
texttexttext
texttext
texttexttext




Example: third party devices:


Examples of improper networks Do NOT do this:

Unterminated cable:

Incorrect location of termination resistor:


Multiple cables in a star configuration


Backbone cable with long stubs:

Schneider Electric Nigeria

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.