{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a deeper version of the AR7711?
Issue:
The PDU needs to be mounted deeper than AR7711 allows.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The installation requires a deeper bracket.

Resolution:
There's not a deeper version of the AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to approx. 5.7".
See attached file

Schneider Electric Nigeria

Attachment(s)
20140116 How to Make AR7711 Mount Deeper.pdf [21.23 KB]