{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can one find max line current values for the ATV312 drives?

Issue:
Max line current values for the ATV312.

Product Line:
Altivar ATV312

Environment:
All

Cause:
Input line currents for the ATV312 drives.

Resolution:
The input line supply values are going to be for voltages between 200VAC to 240VAC or  380VAC to 500VAC 50/60hz.
See the ATV312 install manual document bbv46391 page 10 thru 11 for line current max values.
https://www.se.com/ww/en/download/document/BBV46391/

Schneider Electric Nigeria