{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Vijeo Designer link to individual bits from an INT or DINT using the RSLogix 5000 L5K file?
Issue
Does Vijeo Designer link to individual bits from an INT or DINT using the RSLogix 5000 L5K file?

Product Line
Vijeo Designer

Resolution
When using the Vijeo Designer Link Variable feature to link RSLogix5000 *.L5K file, one will only be able to import the tags that are declared in the Logix application and not the bit extraction of the tag.

The work around would be to manually create those tags as new Variables in Vijeo Designer.

To extract that bit, you will have to manually create the tags in Vijeo Designer as Program:MainProgram.tagname.x as the Device Address (where x is the bit 0 to 15 location for a program scope tag).

Schneider Electric Nigeria