{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to release latched contacts on the VAMP 321 relay

Issue
The protection elements are set to latch upon initialization and they need to be reset.

Product Line
VAMP 321

Resolution
The contacts may be released from the front screen of the VAMP 321 or from VAMPset. From within VAMPset navigate to the RELEASE OUTPUT MATRIX LATCHES screen then set Release Latches to Release and write the changes to the VAMP 321 relay.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: