Search FAQs
Can I connect a USB Barcode Scanner to a HMISTU655/855?
Issue:
Can I connect a USB Barcode Scanner to a HMISTU655/855?
Product Line:
HMIS5T, HMISTU655, HMISTU855
Resolution:
The HMISTU655/855 USB port does not have enough power to fully power up the USB Barcode scanner.
Your two options would be to use a USB hub that have an external power or use the advanced panel Magelis that have enough power on the USB port.
Can I connect a USB Barcode Scanner to a HMISTU655/855?
Product Line:
HMIS5T, HMISTU655, HMISTU855
Resolution:
The HMISTU655/855 USB port does not have enough power to fully power up the USB Barcode scanner.
Your two options would be to use a USB hub that have an external power or use the advanced panel Magelis that have enough power on the USB port.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: