Issue:
ATV212 use with SoMove.
Product Line:
Altivar 212
Environment:
All serial numbers
Cause:
Customer wanted to use SoMove to program ATV212, but the ATV212 was not listed in the SoMove device options.
Resolution:
SoMove should work with the ATV212 drive, if the ATV212 Drives firmware is V5.1 or higher.
Link to Somove and DTMs: https://www.se.com/us/en/product-range/2714-somove/#software-and-firmware
Released for:Schneider Electric Nigeria