{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find the part number, serial number & firmware version on the ATV61 and ATV71 drives?

Issue:
Confirming the catalog number, serial number, firmware version & installed options on Altivar 61 & 71 (ATV61/ATV71) variable frequency drives.

Product Line:
Altivar 61, Altivar 71

Resolution:



Using the HMI display (VW3A1101), you can find the catalog number for the drive in the Identification Menu, 1.11.  The path is Drive Menu > 1.11 Identification.  The top line in this menu shows the drive catalog number.

You can also find the part number and serial number on the nameplate.  The nameplate is a silver sticker located on the right side of the drive itself.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria