{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are there 21" mounting rails available for the NetShelter cabinets?

Issue:
21" wide mounting rails are required for a NetShelter cabinet.

Product Line:
NetShelter

Environment:
All versions and serial ranges.

Cause:
Some telecommunications equipment is manufactured to ETSI standards which can require 21" wide mounting rails. This is not a current EIA/ECA-310-E width.

Resolution:
There is currently no 21” mounting rail kit available as an accessory for the NetShelter cabinets. The 21" width does not exist in the EIA/ECA-310-E specification. It comes from the the ETSI (European Telecommunication Standards Institute) standard, which  allows for 19”, 21” and 23” mounting rail widths. If the opportunity involves 100 or more cabinets with 21" wide rails we can investigate a custom cabinet request. Please contact your APC supplier or sales rep to pursue a custom cabinet request.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: