Search FAQs
What is the default username and password for ION/SPM/PME components?
Issue
What is the login credentials for ION/SPM/PME components
Product Line
ION Enterprise
StruxureWare Power Monitoring
Power Monitoring Expert
Environment
Schneider Electric Power Monitoring Software Applications
Cause
User may not know the default login credentials
Resolution
Note: At version 7.2 and later, there are no longer default user passwords for PME. During installation the password for supervisor user is configurable.
Enter one of the default username and passwords into required fields of each system component.
Username: supervisor
Password 0
or
Username: guest
Password: 0
The access level for the default usernames are:
What is the login credentials for ION/SPM/PME components
Product Line
ION Enterprise
StruxureWare Power Monitoring
Power Monitoring Expert
Environment
Schneider Electric Power Monitoring Software Applications
Cause
User may not know the default login credentials
Resolution
Note: At version 7.2 and later, there are no longer default user passwords for PME. During installation the password for supervisor user is configurable.
Enter one of the default username and passwords into required fields of each system component.
Username: supervisor
Password 0
or
Username: guest
Password: 0
The access level for the default usernames are:
Software Version | Username | Access Level |
ION 5.x | supervisor | Supervisor |
ION 5.x | guest | Supervisor |
ION 6.x | supervisor | Supervisor |
ION 6.x | guest | Supervisor |
SPM 7.x | supervisor | Supervisor |
SPM 7.x | guest | Observer |
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: