{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How does a dirty air / dust filter effect the airflow and influence thermal capacity of a NetShelter CX cabinet?

Issue:
Dirty air/dust filters can negatively effect airflow.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Dirty air / dust filter, needs cleaning.

Resolution:
When a NetShelter CX is fitted with a set of dust filters it is expected that the airflow will be reduced by 3%. This will have very little effect on the thermal capacity of the cabinet.
But, if the amount of dust collected by a set of filters is greater than 0.8 grams on a AR4018 or AR4024-series or 1.6 grams on a AR4038-series, then the thermal capacity will be reduced by at least 10 %. 
To avoid this it's recommended that dust filter is cleaned at regular intervals.

Attached below please find the complete test report.  
 

Schneider Electric Nigeria

Attachment(s)
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.