Search FAQs
What is the thickness of the Steel sheet metal used in Okken switchboard.
The Steel sheet metal thickness used in Okken switchboard is as listed below:
Okken Steel sheet metal thickness
Okken Steel sheet metal thickness
Housing | Thickness mm |
Door | 2.00mm |
Rear panels | 1.50mm |
Side panels | 1.50mm |
Roof | 1.50mm |
Inter Cubicle | 1.50mm |
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: